2017-02-13 11:28 PM
Hi All,
I am using SPC560B-Discovery board,
SPC Studio Version: 5.2.1
I want to configure WKUP[2](Pin Number :PA[1]) as external wake up source,
I didn't find any call back function code generation for wake up using Code Generator,
I am expecting there should be some way to generate code for wake up call back function,Same as how we are generating code for EIRQ call back function using Code Generator,
whether it is possible to generate call back function for Wake-up sources same as EIRQ,
If possible please guide me how to generate the Wake up call back code,
If not possible to generate code for wake-up source using Code generator,
Please provide me some sample code to configure external wake source (Example : when switch press,system should wake up)
Thanks in advance,
---
Thanks & Regards,
Mujeeb.
Solved! Go to Solution.
2017-02-14 5:20 AM
Hello Mujeeb ,
There is some example in the application wizard
https://community.st.com/0D50X00009XkYJySAN
Best Regards
Erwan
2017-02-14 2:42 AM
Hello
I have moved your question to the
https://community.st.com/community/automotive-mcus-community/spc5-automotive-mcus
forum where someone should be able to assist you.Thanks
Oli
2017-02-14 5:20 AM
Hello Mujeeb ,
There is some example in the application wizard
https://community.st.com/0D50X00009XkYJySAN
Best Regards
Erwan
2017-03-02 10:53 PM
Hi Erwa,
Thanks for your replay,
this is Timer based example,
I would like to know how to configure wake up pin using SPC code configurator,
Example : We are configuring EIRQ and respective call back using code generator
same way is it possible to generate code for wake up pin if it is possible how?,please guide how to do that,
my main requirement is when ever any external interrupt comes(EIRQ example : Switch pressed) my system should wake up,
Wake can be configured as EIRQ is it possible ?
---
Thanks & Regards,
Mujeeb
2017-03-03 2:32 AM
Hello Mujeeb ,
Step 1 : You have to use the Pinmap to configure the WKUP.
Step 2 : Plug your button with the WKUP pin
Step 3 : Enable PCTL WKUP
it is better to your function to wakeup in SRAM
i will send you an example application already coded in previous posts.
Best regards
Erwan
2017-03-13 12:31 AM
Hi Erwan,
Thanks for your replay,
Can you please provide the sample code ,
I have tried configuring as you suggested ,but how to configure call back function ,can you please help us to solve this issue
---
Thanks & Regards,
Mujeeb Shaik.
2017-03-13 4:31 AM
Hello Mujeeb ,
You can grab the example code from the application wizard in SPC5Studio (RLA or HAL)
SPC560Dxx OS-Less WKPU LPM Test Application for Discovery
SPC560Dxx_RLA WKPU API Test Application for Discovery
Best regards
Erwan