2019-09-25 03:19 AM
We are designing a board with the SPBTLE-1S as a network module connected by the SPI port with a STM32L072 as a host.
We would like to have an output interrupt when there are new SPI data from the module.
We would also like to put the module in deep_sleep.
Thank you in advance
2019-10-02 12:41 AM
Please check STSW-BlueNRG1-DK v3.1.0:
located in BlueNRG-1_2 DK 3.1.0\Project\BLE_Examples\DTM