Can the STUSB47xx renegotiate a power contract under processor control?
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-09-26 8:02 PM
I'd like to build a multi-port USB-C charger that allocates higher wattage to recently-plugged-in-devices. (Say a 30W charger that will provide 9V@2A for the first device, but then scale back to 5V@3A for each if two devices are plugged in)
To do this, I'd like to control the power offerings from a processor. Is there a way I can force a connected 47xx to redo power renegotiation with new PDOs ?
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0