cancel
Showing results for 
Search instead for 
Did you mean: 

Can we have the source of the DTM_SPI project for the SPBTLE-1S module?

julius_21
Associate II

We are designing a board with the SPBTLE-1S as a network module connected by the SPI port with a STM32L072 as a host.

We would like to have an output interrupt when there are new SPI data from the module.

We would also like to put the module in deep_sleep.

Thank you in advance

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Winfred LU
ST Employee

Please check STSW-BlueNRG1-DK v3.1.0:

https://www.st.com/content/st_com/en/products/embedded-software/evaluation-tool-software/stsw-bluenrg1-dk.html

located in BlueNRG-1_2 DK 3.1.0\Project\BLE_Examples\DTM