cancel
Showing results for 
Search instead for 
Did you mean: 

Wake up from STANDBY0 and HALT0 mode in SPC58EC80 eval board

RSeba.2
Associate III

How to wake up from STANDBY0 mode and also Halt0 mode?

Is it possible to wake up or come out of STANDBY0 mode by pressing the reset button on the eval board?
I tried it that way, but it is responding to the reset.

RSeba2_0-1706604928623.png

As mentioned in the table above, can a system reset (hardware reset) be used to wake up from HALT0 and STANDBY0 mode?

0 REPLIES 0