2015-01-19 01:45 AM
Hello,
I am trying to build a project created using SPC5Studio Wizard. The steps used are File->New->SPC5Studio Wizard. Afte this I selected SPC560D-DIS as the product line. Then selected all the drivers with OSLess version. I selected all the available applications for this configuration. I tried building one of the application - SPC560Dxx OS-Less Test Application for Discovery, it is giving following errors,- Symbol 'NULL' could not be resolved- Symbol 'uint32_t' could not be resolved- Symbol 'int32_t' could not be resolved- Symbol 'uint16_t' could not be resolved- Symbol 'uint8_t' could not be resolvedSimilar errors for different defines used in main.c file are there. Few errors are for the functions used like osalThreadSleepMilliseconds().Can you please help me resolve these? Is any project setting/configuration missing?Your earliest help in this regard will be highly appreciated.Thanks in advance for all your help.Mike. #virtual-timer #virtual-timer #spc5studio-build #spc56-examplesSolved! Go to Solution.
2015-02-25 06:31 AM
Hello Mike ,
Your application does not come from the application wizard ''SPC5Studio 3.4.2''. OSAL Components have been updated from 3.2.X. (API Function osalVTSetI by VTSetI) 2 choices : 1) if you have not important settings : Remove this application and reimport it from the application wizard. 2) if you have some personal settings on CAN : export it to save it, Remove this application and reimport by the application wizard (cf attachment) it should work 😉 Best regards Erwan ________________ Attachments : 2015-02-25_153024.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWSz&d=%2Fa%2F0X0000000boH%2FBtRAW8an6SMPQ_NAa3yTu9siGFj8lHjEJVQgoMkNZKI&asPdf=false2015-02-26 01:37 AM
Hello Erwan,
I tried using test application imported using Application Wizard for v3.4.2. Still the issue for 'osalVTSetI' remains. Please find attached project. Thanks. Mike. ________________ Attachments : SPC560Dxx_OS-Less_CAN_Test_Application_for_Discovery.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qYZ3&d=%2Fa%2F0X0000000bp3%2FZl2tivAwexkWgEWuLSmJCRSFyhYHqGhK17PBs1_Y3SY&asPdf=false2015-02-26 02:10 AM
Hello Mike ,
you use a ''deprecated'' AppWizard not compliant for SPC5Studio 3.4.2 Could you confirm your installation details ? Help ==> About SPC5Studio ==> Installation Details (Cf Attachment) When there is a release, for the update site , you should update all the features (SPC5Studio Core , SPC5Studio Appwizard , SPC5-HAL and so on ..) (Cf Attachment) Best Regards Erwan ________________ Attachments : 2015-02-26_110822.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWTw&d=%2Fa%2F0X0000000boI%2F3M3OutL0vDA7RYE87IrPhaIAeBsDQWmGwlheGeXSwPk&asPdf=false2015-02-26_110923.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWlH&d=%2Fa%2F0X0000000boW%2F_S2U0aQ7ooa.X9UpMdIjjyBBE0xWNHAlIjzaP_2mQ_M&asPdf=false2015-02-26 02:58 AM
PFA - Installation Details
I have updated the SPC5Studio using 'select all' option only. Thanks. Mike. ________________ Attachments : Installation_details.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qXCc&d=%2Fa%2F0X0000000bog%2F1j9ZUDj618MmFmyEorZ1MXRSSWDLFPtd1xSLNMry5ys&asPdf=false2015-02-26 05:02 AM
Hello Mike ,
Have you still your compilation issue ? Did you remove the application from your workspace and use the Application Wizard ? (Cf Screenshot) Best regards Erwan ________________ Attachments : 2015-02-26_140105.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0YB&d=%2Fa%2F0X0000000baO%2Fu_Cb2X1HvlSsOYF6CG6Jo9G9V0e.NqaZm9FYUhAH1N4&asPdf=false2015-02-26 05:41 AM
Yes Erwan. I did remove the application from my workspace and used App wizard to include the new test application. Still facing the issue.
Mike.2015-02-26 06:33 AM
2015-03-08 11:04 PM
Hello Erwan,
It worked after changing the workspace. Can you please clarify the issue/problem so that in future whenever new release is installed, I cam take care of it.Thanks.Mike.2015-03-09 01:38 AM