2024-07-15 03:14 AM
Hello,
I am trying to run Projects\System\SIUL2\siul2LedBlink from StellarSDK_4.0.0 on a SR6G7EVBC4000P_RevA board. The project was successfully build.
To flash the board in RAM, I am using the last version of Lauterbach. When running, it seems that it can't break on main.
For testing purposes, I was running the sieve_ram_aarch32_arm_v8r_le.elf using the same Lauterbach script and the execution and breaking on main was done as expected. On a deeper investigation, I have found out that the .elf file form Lauterbach differs from the one build. Those differences can be seen below.
Also, I have tried running an example from Lauterbach using the NVM, but I get the following error:
Do you have any suggestions to run Projects\System\SIUL2\siul2LedBlink on the board? Also, to flash an application on NVM and fix the flash programming error.
Thanks in advance :grinning_face:
2024-07-15 07:00 AM
Hello ,
I am checking with Local FAE and SDK SR6
Best regards
Erwan