2019-11-18 06:32 AM
Dear All,
I work with SPC56EC64 and have a question about debugging.
For debug, I use SPC5-UDESTK debugger. Now I can't access a flash. During programming popped communication error. Since I can't access the flash memory to read or write. If I configure Target without the flash, I access RAM and Core register. But I can't connect Target if flash handling is enabled. In the datasheet, I read about shadow flash and similar. I guess I can erase the shadow flash and now I have no access to it.
Is there a possibility to access the flash?