cancel
Showing results for 
Search instead for 
Did you mean: 

No access flash after programming (SPC56EC64)

BViktar
Associate

Dear All,

I work with SPC56EC64 and have a question about debugging. 

For debug, I use SPC5-UDESTK debugger. Now I can't access a flash. During programming popped communication error. Since I can't access the flash memory to read or write. If I configure Target without the flash, I access RAM and Core register. But I can't connect Target if flash handling is enabled. In the datasheet, I read about shadow flash and similar. I guess I can erase the shadow flash and now I have no access to it. 

Is there a possibility to access the flash?

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0