2023-04-21 07:12 AM
2023-04-21 07:57 AM
Hello,
the graphical clock tree is not existing on all SPC5xx devices, which SPC5 MCU do you use ?
Best Regards.
2023-04-21 08:12 AM
Hello,
I am using SPC560P MCU !
2023-04-21 08:13 AM
Hello,
I am using SPC560P MCU !
2023-04-21 08:13 AM - edited 2023-11-20 07:29 AM
We do not have graphical clock tree for these 3 products:
SPC572Lxx
SPC574Sxx
SPC58xExx
But you can configure with the textual clock component:
2023-04-21 08:24 AM - edited 2023-11-20 07:30 AM
2023-04-21 08:29 AM
Can you help me see if I'm using SPC56P that doesn't show up !
2023-04-21 08:35 AM - edited 2023-11-20 07:30 AM
Do you have same MCU than me ?
2023-04-21 08:35 AM - edited 2023-11-20 07:30 AM
2023-04-21 08:38 AM
would you please:
1) close SPC5Studio
2) erase .log file in C:\SPC5Studio-6.0\workspace\.metadata
3) open SPC5Studio
4) reproduce the issue
5) provide me the new .log file