cancel
Showing results for 
Search instead for 
Did you mean: 

I don't understand why in SPC5Studio in "SPC5 RLA IRQ Component" in ISR section it is possible to set the interrupt priority up to 15. In SPC58EC80E5 it is written that the priority level can be up to 64 (0 to 63). Can someone help me? Alessandro

AParm.1
Associate II
 
1 ACCEPTED SOLUTION

Accepted Solutions
zambrano.luigi
Senior III

Hi,

you are right. We will fix it in the next releases. As temporary workaround, you can fix it by changing manually the priority in the file irq_cfg.c just after the SPC5Studio code generation.

Regards,

Luigi

View solution in original post

3 REPLIES 3
AParm.1
Associate II

Please, there is someone that can help me regarding the question above?

zambrano.luigi
Senior III

Hi,

you are right. We will fix it in the next releases. As temporary workaround, you can fix it by changing manually the priority in the file irq_cfg.c just after the SPC5Studio code generation.

Regards,

Luigi

AParm.1
Associate II

Thank you very much Luigi,

Regards,

Alessandro P.