cancel
Showing results for 
Search instead for 
Did you mean: 

how to flash binary into spc563M-disp board?

arro239
Senior
Posted on July 30, 2014 at 04:54

I've compiled some code & I have .bin/.dmp/.elf/.hex/.map files.

How do I program/flash whichever I need to flash into spc563M-disp board? I do have a PLS device, the driver and UDE Desktop installed.

While AN4425 promises ''The document UM1602 (see Reference documents) is focused to describe and to understand how to use SPC5studio and how to create, build and debug a project.'', I do not see the word ''debug'' mentioned in UM1602 SPC5 Studio users guide even once, but maybe I am doing something wrong.

Please advice.
This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
1 REPLY 1
Erwan YVIN
ST Employee
Posted on July 30, 2014 at 10:23

Hello Andrey ,

To debug the project :

1) Please check if the driver is well installed in DEVICE MANAGER (Cf screenshot)

2) 2 possibilities : (cf screenshot)

Example : on the repository

you need to double-click on ''debug.wsx''

or click on debug button on Activity wizard

In your custom application you need to create a UDE directory like the test applications repository.

With UDE , you will be able to flash and debug.

Best Regards

Erwan

________________

Attachments :

2014-07-30_091154.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qWH2&d=%2Fa%2F0X0000000bo9%2F4xSBxVWULZT8iLmFaSrKHOoguB7Ems__jXSy2Xn4ziE&asPdf=false

2014-07-30_101727.png : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qXcL&d=%2Fa%2F0X0000000bos%2FyHHOwtaAmwlkjXv_YRILV653IIwJZRvLjIVy4X3NvMo&asPdf=false