cancel
Showing results for 
Search instead for 
Did you mean: 

Ethernet comunication example SPC58EC and linux

AMarc.9
Associate

Hi all,

Someone has a working example of simple communication via Ethrnet TCP between linux and freertos with the SPC58EC.

Thnaks in advance

1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee

Yes ,

SPC58ECxx_RLA Network Ping Test Application for Discovery

Have you followed the README.txt

"This application is an example on how to use the FreeRTOS network component.

It needs to configure the network component providing the networking configuration:

i.e: MAC Address, IP static Address.

Open a console and ping from a remote host to the IP address configured for the board.

Fit the following jumpers to configure the network:

JP5:

ETH_PWR  -> [3 - 4]

RESET   -> [5 - 6]

ETH_TX_CLK -> [7 - 8]

ETH_TXD_0 -> [9 - 10]

ETH_TXD_1 -> [11 - 12]

ETH_TXD_2 -> [13 - 14]

ETH_TXD_3 -> [15 - 16]

ETH_TX_EN -> [17 - 18]

ETH_MDIO  -> [19 - 20]

ETH_MDC  -> [21 - 22]

ETH_COL  -> [23 - 24]

ETH_CRS  -> [25 - 26]

ETH_RX_ER -> [27 - 28]

ETH_RX_DV -> [29 - 30]

ETH_RXD_0 -> [31 - 32]

ETH_RXD_1 -> [33 - 34]

ETH_RXD_2 -> [35 - 36]

ETH_RXD_3 -> [37 - 38]

ETH_RX_CLK -> [39 - 40]

JP50: FIT"

View solution in original post

1 REPLY 1
Erwan YVIN
ST Employee

Yes ,

SPC58ECxx_RLA Network Ping Test Application for Discovery

Have you followed the README.txt

"This application is an example on how to use the FreeRTOS network component.

It needs to configure the network component providing the networking configuration:

i.e: MAC Address, IP static Address.

Open a console and ping from a remote host to the IP address configured for the board.

Fit the following jumpers to configure the network:

JP5:

ETH_PWR  -> [3 - 4]

RESET   -> [5 - 6]

ETH_TX_CLK -> [7 - 8]

ETH_TXD_0 -> [9 - 10]

ETH_TXD_1 -> [11 - 12]

ETH_TXD_2 -> [13 - 14]

ETH_TXD_3 -> [15 - 16]

ETH_TX_EN -> [17 - 18]

ETH_MDIO  -> [19 - 20]

ETH_MDC  -> [21 - 22]

ETH_COL  -> [23 - 24]

ETH_CRS  -> [25 - 26]

ETH_RX_ER -> [27 - 28]

ETH_RX_DV -> [29 - 30]

ETH_RXD_0 -> [31 - 32]

ETH_RXD_1 -> [33 - 34]

ETH_RXD_2 -> [35 - 36]

ETH_RXD_3 -> [37 - 38]

ETH_RX_CLK -> [39 - 40]

JP50: FIT"