2021-10-18 09:01 AM
Hi all,
Someone has a working example of simple communication via Ethrnet TCP between linux and freertos with the SPC58EC.
Thnaks in advance
Solved! Go to Solution.
2021-12-01 01:24 AM
Yes ,
SPC58ECxx_RLA Network Ping Test Application for Discovery
Have you followed the README.txt
"This application is an example on how to use the FreeRTOS network component.
It needs to configure the network component providing the networking configuration:
i.e: MAC Address, IP static Address.
Open a console and ping from a remote host to the IP address configured for the board.
Fit the following jumpers to configure the network:
JP5:
ETH_PWR -> [3 - 4]
RESET -> [5 - 6]
ETH_TX_CLK -> [7 - 8]
ETH_TXD_0 -> [9 - 10]
ETH_TXD_1 -> [11 - 12]
ETH_TXD_2 -> [13 - 14]
ETH_TXD_3 -> [15 - 16]
ETH_TX_EN -> [17 - 18]
ETH_MDIO -> [19 - 20]
ETH_MDC -> [21 - 22]
ETH_COL -> [23 - 24]
ETH_CRS -> [25 - 26]
ETH_RX_ER -> [27 - 28]
ETH_RX_DV -> [29 - 30]
ETH_RXD_0 -> [31 - 32]
ETH_RXD_1 -> [33 - 34]
ETH_RXD_2 -> [35 - 36]
ETH_RXD_3 -> [37 - 38]
ETH_RX_CLK -> [39 - 40]
JP50: FIT"
2021-12-01 01:24 AM
Yes ,
SPC58ECxx_RLA Network Ping Test Application for Discovery
Have you followed the README.txt
"This application is an example on how to use the FreeRTOS network component.
It needs to configure the network component providing the networking configuration:
i.e: MAC Address, IP static Address.
Open a console and ping from a remote host to the IP address configured for the board.
Fit the following jumpers to configure the network:
JP5:
ETH_PWR -> [3 - 4]
RESET -> [5 - 6]
ETH_TX_CLK -> [7 - 8]
ETH_TXD_0 -> [9 - 10]
ETH_TXD_1 -> [11 - 12]
ETH_TXD_2 -> [13 - 14]
ETH_TXD_3 -> [15 - 16]
ETH_TX_EN -> [17 - 18]
ETH_MDIO -> [19 - 20]
ETH_MDC -> [21 - 22]
ETH_COL -> [23 - 24]
ETH_CRS -> [25 - 26]
ETH_RX_ER -> [27 - 28]
ETH_RX_DV -> [29 - 30]
ETH_RXD_0 -> [31 - 32]
ETH_RXD_1 -> [33 - 34]
ETH_RXD_2 -> [35 - 36]
ETH_RXD_3 -> [37 - 38]
ETH_RX_CLK -> [39 - 40]
JP50: FIT"