2022-04-16 10:45 PM
Hello
I'm working with spc560p and I want to enable serial receive interrupt, that whenever data received, it save the data and so on.
I could send data by serial driver as sd_dll_write command and its ok. But when I want to use sd_dll_read, actually mcu stopped. It is cleared that I should use interrupt. But need some help.
Thanks
Solved! Go to Solution.
2022-05-16 11:54 PM
Hello,
happy that it works now.
You must set sync to 0 before each time you call sd_lld_read:
if (sync == 1) {
sync = 0;
sd_lld_read(...);
}
Would you please put a best answer if you are happy of my support.
Best Regards,
-Olivier
2022-04-25 05:25 AM
Hello,
you can look at this example "SPC560Bxx_RLA SERIAL DMA Test Application for Discovery"
in low level driver, a RX callback is configured in Low Level Drivers Component->LINFkex Settings->SERIAL configurations
and the configuration structure is given to sd_lld_start in main
Best Regards,
-Olivier
2022-04-26 01:16 AM
Thanks Olivier
2022-05-10 02:35 AM
Hello
I think this interrupt will be enable when the receive was complete. In this case, I can't read my receive buffer. So as the uart protocol is active low, we need interrupt that enable with falling edge.
Would you please interduce me interrupt that would be enable with falling edge?
Thanks
2022-05-13 02:26 AM
Hello,
we have roughly 2 main ways to read on UART driver.
1) In synchronous mode (SerialConfig.api_mode=SPC5_LIN_API_MODE_SYNCHRONOUS)
you call function sd_lld_read(buffer, N) and when it returns, the buffer was fulfilled with N bytes so you can process them.
2) In asynchronous mode (SerialConfig.api_mode=SPC5_LIN_API_MODE_ASYNCHRONOUS)
you configure a callback function in SerialConfig.rx_end_cb = myRXCB;
you reset a global variable sync = 0;
you call function sd_lld_read(buffer, N) and when it returns, the RX process was started but the buffer is empty.
when the buffer will be full with N bytes, your callback function will be called:
void myRXCB(SerialDriver *sdp)
{
sync = 1;
}
after calling sd_lld_read, you must wait your buffer is full before to process it:
while(sync == 0);
Best regards,
-Olivier
2022-05-13 10:17 PM
Hello Olivier
Thanks for your attention and answering. I enabled myRXCB and wrote below code:
void myRXCB(SerialDriver *sdp)
{
(void)sdp;
sync = 1;
while(sync ==1){
pal_togglepad(portD, pad7);
}
}
Or
void myRXCB(SerialDriver *sdp)
{
(void)sdp;
sync = 1;
while(sync ==1){
sd_lld_write(&SD1, 0xAA, 1);
}
}
and I have another mcu as master to send uart code to my spc560.
But in these two case, nothing happened. No led blinks an no 0xAA.
2022-05-16 07:38 AM
Hello,
I would recommend you to not put too much code in the callback function, because it should return as soon as possible and avoit re-entrance calling UART interface (such as sd_lld_write)
at minimum, do never put a while instruction in the callback because you never know how many time you will spend in.
you could just write it like this:
void myRXCB(SerialDriver *sdp)
{
(void)sdp;
sync = 1;
pal_togglepad(portD, pad7);
}
and register this myRXCB into the structure passed as second parameter of sd_lld_start
be sure that your portD and pad7 are well configured and wired to your LED on your PCB
in order to see the LED toggling, you need to wait at least 200ms between two sd_lld_read in your main program:
sd_lld_read(&SD1, ... );
osalThreadDelayMilliseconds(200);
Best regards,
-Olivier
2022-05-16 07:43 AM
Do you use your own PCB ? or do you use one of our Discovery boards ? (SPC56P-Discovery - Discovery Kit for SPC56 P line - with SPC560P50L5 MCU - STMicroelectronics)
2022-05-16 10:01 PM
Hello,
Thanks for your answering, I tried this method and it works correctly. But callback function works once so when sync rest to zero after all, it doesn't work again and callback didn't work as sync = 1 .
So how should it works again an callback put 1 in sync again too?
My code:
void myRXCB(SerialDriver *sdp)
{
(void)sdp;
sync = 1;
}
.
.
.
for(; ;){
if(sync == 1){
sd_lld_read(&SD1, buffer,1);
if(buffer ==0xAA){
pal_togglepad(portD, pad7);
}
sync=0;
}
else{
sync=0;
}
}
2022-05-16 10:02 PM
Hello,
I use my own PCB.