cancel
Showing results for 
Search instead for 
Did you mean: 

Device specific model ''SPC563M64L7'' not supported!

luemy
Associate
Posted on August 07, 2014 at 12:03

Hello community,

i try to use the PinMap wizard in SPC5 Studio 3 and i receive the meassage ''Device specific model ''SPC563M64L7'' not supported!'' and it seems that there is no support for any model cause i try it with different cpu's.

I use the SPC56M- Discovery board and i'm wondering also that this board is not available in the SPC5Studio Application Wizard.

Any ideas?

Thanks for your help!

- Marc
1 ACCEPTED SOLUTION

Accepted Solutions
Erwan YVIN
ST Employee
Posted on September 05, 2014 at 15:39

Hello Marc ,

the pinmap SPC563M64L7 is ready and is available by update site.

You can install it from the web by using the command ''Install new software''

    Best Regards

                     Erwan

View solution in original post

4 REPLIES 4
Erwan YVIN
ST Employee
Posted on August 07, 2014 at 13:34

Hello Marc ,

SPC5Studio is supported SPC563M64L7 .

But, the pinmap wizard for SPC563M64L7 is not ready at the current time.

it should be available in the following weeks.

(Please check your update site)

SPC56M- Discovery board is not available on Application Wizard.

Anyway, if you want to be compliant with SPC56M- Discovery, you can update the application SPC563Mxx OS-Less test application. (EVB with SPC563Mxx Mini Module)

with good clock settings and update the io settings.

   Best regards

                Erwan Yvin

luemy
Associate
Posted on August 12, 2014 at 11:25

Thanks a lot for the quick answer!

Erwan YVIN
ST Employee
Posted on September 05, 2014 at 15:39

Hello Marc ,

the pinmap SPC563M64L7 is ready and is available by update site.

You can install it from the web by using the command ''Install new software''

    Best Regards

                     Erwan

Error: flash driver 'spc563mxx' not found