cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot run program ''make''

Patriks
Senior
Posted on July 24, 2014 at 12:44

Hello,

I installed SPC5 Studio and everything works fine and then after a view hours of working, i can´t build my project any more. I am always getting following error and i don´t know why:

make -j4 all

Cannot run program ''make'': Launching failed

12:30:14 Build Finished (took 47ms)

I did not change anything in the settings, just using the SPC5 Studio as it is configured after the installation. But this error seems to come up randomly after a while. So i re-installed SPC-Studio several times. After the installation it worked again and I was able to build my projects. But during working on my code a get the same error again and again after a while.

What could be the reason for that error upcoming randomly? I am using the 30days evaluation license from High-Tec.

This discussion has been locked for participation. If you have a question, please start a new topic in order to ask your question
3 REPLIES 3
Posted on July 24, 2014 at 16:49

Hi,

It is a know problem in version 3.0, usually when this happens you just have to restart the SPC5Studio.

The problem cause is known (wrong environment variables setup so make.exe is not found) and we are working on a solution. The fix will be delivered via the SPC5Studio updater as usual.

A workaround is to add manually the following paths at the beginning of the PATH system environment variable:

C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\ppc-ht-eabi\bin;C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.hightec_1.0.0.201306281422\hightec\bin;C:\SPC5Studio\eclipse\plugins\com.st.tools.spc5.tools.gnu_1.0.0.201306281422\gnutools;

Giovanni

Erwan YVIN
ST Employee
Posted on July 25, 2014 at 14:51

Hello Patrick ,

You can find in this attachment in chapter 2) a solutionhow to recover your correct CDT Environment.

Best regards

Erwan Yvin

________________

Attachments :

SPC5Studio_FAQ_configurations_issue_cx389511_1.0_D2.pdf : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006qYP9&d=%2Fa%2F0X0000000boy%2FsWmcN7DTb5t5JaJKuZVqO7oc52hxQ.eVxrUgbjsKcEE&asPdf=false
Patriks
Senior
Posted on July 27, 2014 at 09:01

Hello,

Thank you both for your help. I will try these workarounds when the error raises again.

Best regards,

Patrik