cancel
Showing results for 
Search instead for 
Did you mean: 

About int18 in sample code spc58ec wkpu

tuananh13
Associate II

Hello, I have a question. Regarding waking up the system from LOW POWER mode, I want to use the WKPU but not with a push button as in the example.  Instead, I want to use a GPIO port to monitor an external signal. I want to use a rising edge interrupt. I cannot use INT18 because it is connected to a push button and the signal pin is always connected to VCC.  Therefore, a rising edge cannot be achieved.

2 REPLIES 2
Erwan YVIN
ST Employee

Hello Tuan,

I recommend to check SPC5Studio Tools Suite

ErwanYVIN_0-1719824281203.png

SPC5-STUDIO - Code Generator, Quick resources configurator and Eclipse development environment for SPC5 MCUs - STMicroelectronics

Which family do you use?

         Best regards

                     Erwan

 

 

 

tuananh13
Associate II

dear Erwan
Thank you very much, I have found the solution.