2021-12-20 11:40 AM
Hello,
I would like to know about the integration between Nucleo-L496GZ with X-Nucleo-IKS01A2 sensor board.
Is there really no example that facilitates the integration of these boards?
There really is no example using the Nucleo-L496ZG integrated with sensors? Anything I want to do with this core should I build from 0?
It's my first time using STM32 and from what I'm realizing I bought the product with the least amount of examples and integrations.
Are there any plans for updates to insert examples of integration of Nucleo-L496ZG with sensor boards? Or do they have a tutorial that facilitates the implementation of the integration?
Thank you.
Solved! Go to Solution.
2021-12-22 01:52 AM
Hi @GThab.1 , in the absence of already-built examples, probably the easiest way to deal with this is to start from the FP-SNS-ALLMEMS1 examples for the STM32L476RG-Nucleo board, and then change the according to the difference in the pinout between the two microcontrollers / X-Nucleo.
Not starting from zero, but at least with a reference framework.
-Dk
2021-12-22 01:52 AM
Hi @GThab.1 , in the absence of already-built examples, probably the easiest way to deal with this is to start from the FP-SNS-ALLMEMS1 examples for the STM32L476RG-Nucleo board, and then change the according to the difference in the pinout between the two microcontrollers / X-Nucleo.
Not starting from zero, but at least with a reference framework.
-Dk