2021-03-03 8:17 AM
Solved! Go to Solution.
2021-03-03 9:47 AM
the typical power consumption increase of the sensor when the MLC is used is in the range of few uA, which is almost negligible compared to the power consumption of the inclinometer itself which is in the range of 400uA, and of a microcontroller which, depends of course on the application, but is at least in the range of tens of uA
2021-03-03 9:47 AM
the typical power consumption increase of the sensor when the MLC is used is in the range of few uA, which is almost negligible compared to the power consumption of the inclinometer itself which is in the range of 400uA, and of a microcontroller which, depends of course on the application, but is at least in the range of tens of uA