cancel
Showing results for 
Search instead for 
Did you mean: 

Which features can be applied on data collected by the inclinometer ?

Pasi MYLLYMAKI
ST Employee
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Carlo LARGHI
Associate III

available features are mean, variance, energy, peak to peak, zero crossing, maximum, minimum and they can be computed on a windows up to 255 samples. You can refer to the application note AN5536 for more details

https://www.st.com/resource/en/application_note/dm00722184-iis2iclx-machine-learning-core-stmicroelectronics.pdf

View solution in original post

1 REPLY 1
Carlo LARGHI
Associate III

available features are mean, variance, energy, peak to peak, zero crossing, maximum, minimum and they can be computed on a windows up to 255 samples. You can refer to the application note AN5536 for more details

https://www.st.com/resource/en/application_note/dm00722184-iis2iclx-machine-learning-core-stmicroelectronics.pdf