it is an high end product, so it is in some dollars range. For an exact price in small qty refer to the website of the distributors since both the IIS2ICLX and its evaluation tools are fully available on the market. For higher quantities it is sugges...
the answer to this question is not straightforward, it really depends on which are the boundary conditions of your application (like the temperature range, the way you can use the axes of the inclinometer, the kind of calibration that you could affor...
ST has already accurate 3-axis inclinometer in its portfolio (IIS3DHHC), but it is not delivering the same superior accuracy and features of the new IIS2ICLX. A further evolution of IIS2ICLX, with 3-axis, is in R&D
In monitoring of structures with an accelerometer there are two main parameters which are of interest: - first one is the measure of any small change of inclination/position overtime, - for example of beams - and this is accomplished by the inclinom...
the usage of high-end ceramic package allows the sensor to be much less sensitive to thermo-mechanical stresses and so to deliver better accuracy and repeatability over temperature and time