VL53L1X range status register stuck at 9
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-07-29 3:21 AM
Hello all, I'm using VL53L1X sensor through the light API.
After the init procedure I can read the correct distance but I read the range status register = 9
in the manual the only allowed range are: 0, 1, 2, 4, and 7
Can someone explain what it means range status = 9 and how to fix it?
BR
Andrea
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-08-21 8:04 AM
Hello all,
it's very difficult to use a I2C sensor without know what the register are used for.
Now I'm running the example and the register #define GPIO__TIO_HV_STATUS 0x0031
is set to 3.
from the comment bit 1 is set when interrupt occurs.
What bit 0 is used for?
Are there a manual with the registers explanation?
BR
Andrea