cancel
Showing results for 
Search instead for 
Did you mean: 

V6180X sometimes does not function on power up or being moved

andrew_henseleit
Associate II

I am using the V6180X Satel boards and occasionally when I power up the sensor it remains non-functional until I pull power, wait 20-30 seconds, and power back up. I've also noticed it sometimes happens when the sensor is moved while operational as well. Is there anyway to tell if this chip goes non-functional (other than the obvious reset power off of a timer)?

0 REPLIES 0