2019-04-02 08:59 PM
2019-04-08 03:49 AM
hi mark, could you please share the screen of the error? It seems it cannot see the USB port of the X-Nucleo... Did you downloaded and installed all the drivers (STSW-LINK009, etc)? Regards
2019-04-08 12:46 PM
2019-04-08 04:26 PM
2020-02-16 09:23 AM
@MDaws have you resolved this issue?
You did not say what code you are running (or I did not see it) on the target. I assume you are running X-Cube-Mems1.
On the Unicleo-GUI web page (https://www.st.com/en/embedded-software/unicleo-gui.html) it says:
"...GUI for X-CUBE-MEMS1..."
I am not sure how "picky" the Unicleo-GUI is. (I am having problems with it connecting to some targets and not others. Look here in this st.com thread: https://community.st.com/s/question/0D50X0000C8elW6SQI/stmicros-unicleogui-pc-application-breaks-when-connecting-through-stmicros-stlink-incircuit-debugger-and-programmer-pod-why) But I am fairly sure if it does not "see" the correct responses from the X-Cube_Mems1 code, it will not connect.
2023-05-03 02:41 AM
Same issue here, in Win10, Unicleo doesn't like to talk to some boards (ex: L476RG, G071RB) but will work nice with others (G0B1RE). Tried everything, including erasing and reinstalling everything Keil-related, ST-related, etc, in this computer, with or without VCP, with or without drivers, with drivers from ST-Link, etc. Now, in the same computer, same OS, we have VirtualBox, and spawned a Win7 OS running like guest system (under Win10 host) - we installed Unicleo and ST-Link drivers in Win7 (including VCP, which is needed for win7, but not for 10, according with ST) and everything works magically, albeit in the host system, they still don't... Mystery.... We gave up Unicleo and are going to write our own toy to rotate that teapot... :P