2023-06-01 5:56 AM
Hi,
I am using a STEVAL-MKI109V3 mother board to evaluate 2 accelerometers :
I want to use the GUI software UNICO v9.14.6.0 but when I want to connect my device, an error popup appear : "ERROR : The adapter board has not been recognized. The WHO_AM_I register value does not match the device selected".
I have updated the motherboard firmware with the v3.48.3 but I still have the problem with my 2 MEMS boards ...
Can someone help me ?
Solved! Go to Solution.
2023-06-07 5:35 AM - edited 2023-11-20 4:13 AM
Hi @thomas Zapparrata ,
You have to change the jumpers' position as I indicated you in the picture below:
If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster.
2023-06-05 5:31 AM
Ciao @Thomas Zapparrata ,
Welcome to ST Community!
Can you send me some screenshots of each step you perform?
Thanks
2023-06-07 1:28 AM - edited 2023-11-20 4:12 AM
Hi @Federica Bossi ,
Thank's for helping me.
Here is the steps I followed :
I hope my explanations are clear.
Thank's in advance for your help.
2023-06-07 5:35 AM - edited 2023-11-20 4:13 AM
Hi @thomas Zapparrata ,
You have to change the jumpers' position as I indicated you in the picture below:
If this solves your problem, please mark my answer as "Best Answer" by clicking on the "Select as Best" button, this can be helpful for Community users to find this solution faster.
2023-06-07 5:44 AM
It is working now, thank's for your help :)
2023-07-07 8:16 AM
I have exactly the same problem but with the LSM6DSV16X (STEVAL-MKI227KA). I can´t see the image of the solution posted.
Can I get some help?
2023-07-07 10:51 AM
It is working now, thank's anyway
2023-07-19 9:36 AM
@Federica BossiCan anyone see the picture? I can't. I have been having this problem over and over again. I am using a STEVAL-MKI109V3 and a IIS3DWB sensor. I have been having the same problem since I bought the sensor. Usually, the problem solves itself by just removing and putting back again the socket onto the development board. However, I have had situations where no matter how many times I plug and unplug the problem won't go away. While the problem is happening, if I plug another sensor (IIS2DH) it works just fine. I have already updated the firmware twice. Can you please tell me a solution for this problem? I have add situations where I wasn't able at all to use the sensor and a day after it works fine. It is really not reliable at the moment. Thanks in advance.
2023-09-26 11:21 AM
Hello @Eduardo1 ;
I am encountering the same problem with regards to the same board. I would greatly appreciate it if you could kindly share the solution you have found to resolve this issue.
2023-09-26 11:46 PM