2020-10-28 02:26 AM
I want to use an accelerometer to calculate the speed of a moving vehicle. For this i need a accelerometer which should give _ve values(2's complement) in Deceleration and +ve values in (2's complement) in acceleration. It should have 2g range with 12bit(or more) resolution. with less noise affected. It should have less Zero offset error.
If there is any sensor Please Suggest me one.
Thank you in Advance.
Solved! Go to Solution.
2020-10-28 03:01 AM
Hi @NMale.1 ,
connecting this post to this thread.
One of the accelerometers with low noise available in ST portfolio is the LIS2DW12, that can operate in high performance mode, 14-bit, with about 100 ug/sqrt(Hz) noise.
I suggest you to compensate an eventual residual initial offset acting on X_OFS_USR (3Ch) to Z_OFS_USR (3Eh) registers.
-Eleon
2020-10-28 03:01 AM
Hi @NMale.1 ,
connecting this post to this thread.
One of the accelerometers with low noise available in ST portfolio is the LIS2DW12, that can operate in high performance mode, 14-bit, with about 100 ug/sqrt(Hz) noise.
I suggest you to compensate an eventual residual initial offset acting on X_OFS_USR (3Ch) to Z_OFS_USR (3Eh) registers.
-Eleon