2019-04-06 8:44 PM
Please help:
I had STSW-MKI109W with STEVAL-MKI196V1
Not Recognize the board on Windows 10
Device manager shown:
What is the driver for my Windows 10
Thanks
2019-04-08 1:20 AM
Hi davidle, if your are using STSW-MKI109W you shuold use the associated tool Unico-GUI (at this link, sw version 8.0.0), not the Unicleo-GUI (which I guess you are using since the version number). The associated hardware tool for Unico-GUI is the STEVAL-MKI109V3, with the standard DIL24 socket for your STEVAL-MKI196V1 (LSM6DSO sensor). There should be no issue with win10 drivers.
Btw, if you want to use Unicleo-GUI, you should associate it to the X-NUCLEO-IKS01A2 expansion board hardware.
Regards
2019-04-08 11:45 AM
Must hold the BT2 and plug the USB cable to the PC to update FW
Then Use New Unico Version 8.0.0
It works!!!
2019-04-08 11:56 PM
Good!