2022-12-08 3:12 AM
I wanna do a live audio processing project and I got an X-NUCLEO-CCA02M2 expansion board with the integrated mics as it says it's compatible with all STM32 boards. However, the pins seem misaligned, i.e. i can't just plug it nicely on top as shown in the manuals or tutorials. Am I missing something? Is there some nonstandard way of connecting those two particular modules together?
Solved! Go to Solution.
2022-12-12 2:07 AM
Hello @HMaje.1,
To connect an X-NUCLEO-CCA02M2 expansion board to a NUCLEO-F746ZG for example development board, morpho header connectors must be soldered on the relevant footprint available on the STM32 Nucleo.
Also, you do not need to solder the whole 2 x 80 pin header but only a pair of 2 x 38 pin stripline connectors as mentioned in Getting started with the digital MEMS microphone expansion board based on MP34DT06J for STM32 Nucleo - User manual
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-12 2:07 AM
Hello @HMaje.1,
To connect an X-NUCLEO-CCA02M2 expansion board to a NUCLEO-F746ZG for example development board, morpho header connectors must be soldered on the relevant footprint available on the STM32 Nucleo.
Also, you do not need to solder the whole 2 x 80 pin header but only a pair of 2 x 38 pin stripline connectors as mentioned in Getting started with the digital MEMS microphone expansion board based on MP34DT06J for STM32 Nucleo - User manual
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
2022-12-12 8:38 PM
Oh, I see, that's unfortunate.
Thank you for a quick response, I'll refer to the materials provided.
Best,
Hubert