2019-05-30 05:09 AM
Hello,
I'm developing a product starting from the WESU eval product. I see on the webpage the pdf with the schematics and the gerber files for production, but unlike other eval boards I cannot find the design project. Could you please provide it? Thank you in advace.
Regards,
Manuel Gómez
2019-05-31 08:32 AM
Hi Manuel, unfortunately the design files for this project are not open. For which application do you need them? I can check if I can find them and share them to you by private mail. Regards
2019-06-02 11:15 PM
Hi Eleon,
We're developing a device for monitoring the quality of the sleep, and we're using the WESU as the central unit with the accelerometer. Now we want to design our own board, with a connector for a second accelerometer in order to extend the capabilities to a double bed. Having the original project would be much easier to replicate the structure, as we won't need to copy the schematics from the PDF files. In case you can find them and share with me please contact me through private message.
Best regards,
Manuel