cancel
Showing results for 
Search instead for 
Did you mean: 

STEVAL-BFA001V1B wrong cable description

MMade.1
Associate II

I wanted to try the STEVAL-IDP005V1 from STEVAL-BFA001V1B,

I followed the description given in UM2438

and nothing worked,

Finally I realized that the cable description is wrong (or may be I've got a bad cable),

the ground is on white, not on blue wire

5 REPLIES 5
iNav
Associate II

your right.

White is GND. The document description is different than actual wiring.

Do you feel lot of heat generated around Accelerometer?

MMade.1
Associate II

yes, I feel heat too, a little warm, but it is normal, I think it is coming from MCU on other side, BR

AmrithHN
Associate III

Are you sure about this? I have

STEVAL-BFA001V1B and it has 4 wires for io link as per the user manual

blue is GND and grey is +VCC (18-24V) 

I tried this and I was able to get the mcu and UART to send me the starting message with some details.

 

 

How did you verify this? is it available in the schematics?

AmrithHN
Associate III

You got a bad cable documentation is correct and it is supposed to be the same but you might have faulty cable , wired incorrectly