2022-10-24 12:46 AM
When I connect the sensortile.box to the ST BLE Sensor App,
it automatically prompts me to upgrade the sensortile.box's firmware to v349.bin.
As I asked before, if the firmware of the sensor tile.box is upgraded to v3.4.9, the data from the accelerometer cannot be read properly. Vibration monitor demo app does not run properly also..
As a result of inquiring on the ST community site, ST saids that the firmware of the sensor tile.box will be upgraded to v3.4.10 soon.
I hope that all these problems will be cleared if I upgrade the firmware of the sensor tile.box FW to v3.4.10.
By the way, when will the firmware v3.4.10 will be released?