2020-06-01 6:07 AM
Hello,
I have multiple VL6180X sensors which are handled by i2c multiplexor. Once I power up the sensor and configure it I can get measurements, but after MCU reset or switch the power I cannot get new measurements anymore. And the same problem with all other sensors - at first boot all is okay, and after re-power - no new measurements. I don't use GPIO0 for hw reset. Can I reset the sensor via software?
Thanks.