cancel
Showing results for 
Search instead for 
Did you mean: 

Signal delay MEMS Studio BUG

aesteban
Associate III

I think signal delay library does not work on MEMS Studio.

I made an example code to show temperature values from a nucleo-L476RG and x-nucleo-IKS01A3 setup.

The code should show the actual value and a delayed one:

aesteban_0-1715168691138.png

But it gives the following error:

aesteban_1-1715168772554.png

This exact situation was replicated on AlgoBuilder software and worked without any issue.

 

Any idea how could I work this out?

Thanks in advance

1 ACCEPTED SOLUTION

Accepted Solutions
Miroslav BATEK
ST Employee

Hello @aesteban 

indeed it is issue in the Signal Delay function block. We will fix it in the next version of MEMS Studio.

For now you can apply attached patch. Just replace the signal.json file in you MEMS Studio installation folder (c:\Users\USERNAME\AppData\Local\STMicroelectronics\MEMS Studio\release\Library\) by the one in attachment.

 

View solution in original post

1 REPLY 1
Miroslav BATEK
ST Employee

Hello @aesteban 

indeed it is issue in the Signal Delay function block. We will fix it in the next version of MEMS Studio.

For now you can apply attached patch. Just replace the signal.json file in you MEMS Studio installation folder (c:\Users\USERNAME\AppData\Local\STMicroelectronics\MEMS Studio\release\Library\) by the one in attachment.