cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile Box- Steval Mksbox1V1

ShivaRagu
Senior

Hi,

Am trying to generate the C-code for the ASC (Acoustic Scene Classification) model from the FP-AI-SENSING1 Pack through Stm32cube mx. But I can see there is changes in the code between existing code and the new code which was generated by me. I dont know whether I have not done the correct procedure in MX.

It would be really helpful, if I get some procedure for SensorTile Box (Steval-Mksbox1v1) for the ASC to work in MX, because I can see some of the tutorial videos and data briefs is for the eval board " B-L475E-IOT01A1" not for sensor tile box.

As per my understanding, If am generating the C-code from the model from FP-AI-SENSING1, I should get the same code which is already in function pack.

Regards,

shankari.

11 REPLIES 11

hi, I understood, the code change is because of the Version Problem. Now, its working.

Regards,

shankari.

niccolò
ST Employee

Hi shankari @ShivaRagu​ ,

I'm glad you could find the issue

let's keep up the good work with your project

Niccolò