2021-05-12 10:29 PM
Hi,
Am trying to generate the C-code for the ASC (Acoustic Scene Classification) model from the FP-AI-SENSING1 Pack through Stm32cube mx. But I can see there is changes in the code between existing code and the new code which was generated by me. I dont know whether I have not done the correct procedure in MX.
It would be really helpful, if I get some procedure for SensorTile Box (Steval-Mksbox1v1) for the ASC to work in MX, because I can see some of the tutorial videos and data briefs is for the eval board " B-L475E-IOT01A1" not for sensor tile box.
As per my understanding, If am generating the C-code from the model from FP-AI-SENSING1, I should get the same code which is already in function pack.
Regards,
shankari.
2021-05-22 5:49 AM
hi, I understood, the code change is because of the Version Problem. Now, its working.
Regards,
shankari.
2021-05-25 2:53 AM
Hi shankari @ShivaRagu ,
I'm glad you could find the issue
let's keep up the good work with your project
Niccolò