cancel
Showing results for 
Search instead for 
Did you mean: 

SensorTile.box #NaN: Customize your SensorTile.box box to better fit your application

Eleon BORLINI
ST Employee

SensorTile.box platform allows you to customize your application with an increasing complexity, starting from Entry mode (basic examples upload), Expert mode (change the sensor inputs, setting the desired parameters and functions, and implement a custom interface USB/BLE), Pro mode (deep guided modification and customization of the firmware structure).

From now on, you will be able to change also part of the hardware of the system, starting from the shape of the standard box, to adapt it to your application (wearable, industrial...): this opportunity is important to optimize the positioning of the sensors to minimize the spurious effects (especially for the IMUs and the motion sensors).

  • You can find the CAD files for the standard box (the one you can currently purchase) below attached;
  • Another example is the STEVAL-MKSBOX1V1 Alternative box cover to use as a wearable on the user wrist for 3D Printer (.stl file) that you can download at this LINK, In the Hardware Resources / BOARD MANUFACTURING SPECIFICATIONS section.

Enjoy!

1 REPLY 1
Eleon BORLINI
ST Employee

3D rendering of the modified box (online example)

0693W000000W0NnQAK.png