2018-10-21 01:20 PM
Hi,
Does the iNEMO sensor fusion tool work with accelerometers with larger than +-16g output
2018-10-22 05:06 AM
What you mean by "iNEMO sensor fusion tool"?
2018-10-22 05:40 AM
Hi,
Sure, I'm pretty much new to the ST tool chain. I'd interpreted that the software GUI, iNemo (I'm not sure if that's the software tools name), enabled a developer to select ST components in order to build a custom IMU using code auto generated from the tool.
Have I interpreted that correctly?
Thanks,
Joe.
2018-10-24 02:42 AM
Do you have a link to the tool or screenshot? I'm still not sure if you are referring to an existing tool or you are asking for such a tool?
2018-10-24 02:56 AM
Its called algobuilder
2018-10-24 02:57 AM
2018-10-24 05:26 AM
AlgoBuilder supports only X-NUCLEO-IKS01A2 or SensorTile which utilize sensors with maximum range 16g. Theoretically you could modify the FW to work with other sensor with higher range, but the functionality is not guaranteed.