cancel
Showing results for 
Search instead for 
Did you mean: 

I design a battery powered BT Tag using LIS3DE. I want to detect movement as a trigger to transmit BT beacons. Which mode should be choose if I want to reduce the power consumption.

John KUNG
Associate

LIS3DE connects to BLE IC using I2C Bus and INT pins

Please state the mode according to time before and after the trigger.

Second, if I want to monitor 30 seconds after trigger to double check is it need to transmit BT beacons. May I use LIS3DE FIFO to storage data and just wake up BLE IC at the end to reduce power consumption. Or is there have other solution.

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Miroslav BATEK
ST Employee

You can configure the sensor to ODR=10Hz (CTRL_REG1) with current consumption ~3uA and setup interrupt generator (IG1_CFG) to trigger interrupt if acceleration is higher than threshold (IG1_THS) for certain time (IG1_DURATION).

The FIFO has 32 items, so if you want to store 30s you would need to reconfigure the ODR to 1Hz and enable the FIFO (by a mcu) after the interrupt was triggered.

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.