cancel
Showing results for 
Search instead for 
Did you mean: 

Self test in IIS3DWB

Aalekh
Associate II

What is self-test in IIS3DWB and what is the criteria to indicate pass or fail??

3 REPLIES 3
Federica Bossi
ST Employee

Hi @Aalekh ,

Welcome to ST Community!

The embedded self-test functions allow checking the device functionality without moving it. When the self-test is enabled, an actuation force is applied to the sensor, simulating a definite input acceleration. 

The completed procedure is described in the section 8 of AN5444:

FedericaBossi_0-1705419600036.png

 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.
Aalekh
Associate II

What to do if Self-test data is not in specified range?

Federica Bossi
ST Employee

Hi @Aalekh ,

It means that the self test failed.

Can you share the output values with and without self-test enabled? Which FS did you set? Please note that the values we give are for 2g. 

In order to give better visibility on the answered topics, please click on 'Accept as Solution' on the reply which solved your issue or answered your question.