2025-02-03 02:35 AM
Hello community ,
I am going to do 9 axis sensor fusion (6axis accel and gyro + 3axis magnetometer) and got across to the MEMs-Studio suite. I've bought STEVAL-MKI109D for motherboard and STEVAL-MKI217V1 as the shield. STEVAL-MKI109V3 is out of stock at that time.
I pluged the USB for STEVAL-MKI109D with mounted STEVAL-MKI217V1, but the STEVAL-MKI217V1 isn't recognised but was recognised as STEVAL-MKI197V1 instead. The features of 6axis are fine but I need to test the 3axis mag also.
Here are my software setting.
STEVAL-MKI109D firmware was updated to v 0.8.14
MEMs Studio 1.4.2