2024-01-19 1:44 AM
Hello,
"1/ODR (1 à 200 HZ)" is it the response time of the sensor ?
Thank you
Solved! Go to Solution.
2024-01-19 2:31 AM
Hi @ljm ,
What do you mean with "response time"?
If I understood properly the data is ready every ODR so you can read it every 1/ODR seconds.
2024-01-19 2:31 AM
Hi @ljm ,
What do you mean with "response time"?
If I understood properly the data is ready every ODR so you can read it every 1/ODR seconds.
2024-03-13 11:40 PM
I'm currently using your LPS22DFmodule to measure pressure and I saw in the datasheet that the temperature accuracy is ±1.5 °C (T = 0 to 80°C). My working range is between -15°C and 60°C. Could you please give me the accuracy of this sensor in the range -15 to 65°C?