2020-03-10 12:29 PM
I'm working on a low powered bluetooth prototype that has several power constraints. I'm thinking of using the STEVAL-BCN002V1B design as a reference point and I excluded several unused sensors by my project requirements. Will the default firmware still be able to be uploaded through the 10 pin port?
2020-03-13 09:09 AM
Hi @HChun.1 , you mean you want to work with the platform STEVAL-BCN002V1B but your are not interest in using some of the sensors on that platform? You can do it by don't initializing them in your firmware, because the sensors don't consume much current if they are not initialized and if the SPI or I2C for the data acquisition is not running. Regards