2020-05-11 5:42 AM
2020-05-12 12:12 AM
We mentioned two specific SW packages in our webinar: STSW-STWINKIT01 and the predictive maintenance package called FP-IND-PREDMNT1. These can be found at st.com if you search for the STWIN board. Additional SW package we did not talk about is for the microphones specifically and is called X-CUBE-MEMSMIC1, there are also other SW packages for Azure cloud connectivity or a dedicated SW package for use of cellular expansion board. Another SW repository I would like to mention is hosted at GITHUB STMicroelectronics pages https://github.com/stmicroelectronics. You will find here always up-to-date low level platform independent component drivers for MEMS sensors, also drivers specifically for Linux and Android based embedded systems and also you can find here additional specific SW examples utilizing in details the sensor digital functions , like for example the FIFO in its different modes of operation.