cancel
Showing results for 
Search instead for 
Did you mean: 

SPI not working with LSM6DSL

DRote.2297
Associate II

Hello,

I'm using NUCLEO-L476RG connected to eval board of LSM6DSL. I have checked the physical connection with a DVM and it seems to be correct.

I have generated a very simple project using STM32CubeIDE and trying to read the WHO_AM_I register (code below). I'm using a simple USB logic analyzer and I can see that the data is being output correctly on the MOSI line, but there is no answer on the MISO line. What am I missing here?

uint8_t who_am_I;  // Who Am I
who_am_I |= 0x0f;
 
while (1)
  {
    /* USER CODE END WHILE */
 
    /* USER CODE BEGIN 3 */
	  HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_RESET);
	  HAL_GPIO_WritePin(SPI1_nCS_GPIO_Port, SPI1_nCS_Pin, GPIO_PIN_RESET); //Set SPI CS to low
	  HAL_SPI_Transmit(&hspi1, &who_am_I, 1, 1000);  // Read Who Am I register
	  while(HAL_SPI_GetState(&hspi1) != HAL_SPI_STATE_READY);
	  HAL_SPI_Receive(&hspi1, &pBuffer, 1, 1000);
 
//	  HAL_SPI_TransmitReceive(&hspi1, &who_am_I, &pBuffer, who_am_I, 1000);
 
	  HAL_GPIO_WritePin(SPI1_nCS_GPIO_Port, SPI1_nCS_Pin, GPIO_PIN_SET); //Set SPI CS to high
 
 
	  HAL_Delay(100);
	  HAL_GPIO_WritePin(LD2_GPIO_Port, LD2_Pin, GPIO_PIN_SET);
	  HAL_Delay(100);
  }

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Eleon BORLINI
ST Employee

Hi @DRote.2297​ , can you check the MISO and MOSI line with an oscilloscope, if you are getting something like 00h or FFh? Btw, I suggest you to check the STM32CubeL4 firmware package, both in the folder \Drivers\BSP\Components\lsm6dsl, which contains the LSM6DSL drivers for the STM32L4 MCU family and the folder \Projects\NUCLEO-L476RG\Examples\SPI for checking the correct SPI initialization on NUCLEO L4 platform. Regards

DRote.2297
Associate II

Hi @Eleon BORLINI​ , unfortunately I don't have an oscilloscope. I have a USB logic analyzer - when I use it I see FFh.

I initiated the SPI using STM32CubeIDE, tried few different SPI configurations but the result is always the same. What else can it be?