Yes, this is possible. IIS2MDC is potentially the product which can be considered. It Is important to respect the magnetic field strenght vs. IIS2MDC measurement range, and if the sampling speed is sufficient for particular application (150Hz max) et...
This IO-Link stack ensures communication interoperability with other IO-Link devices, specifically an IO-Link master. In other words, beside the IO-Link compliant hardware (ST products) we added also SW layer through our partner to complete the IO-Li...
There is currently no of the box ready example for that, but we have a solution existing. Please have a look here :https://www.st.com/content/st_com/en/search.html#q=BLEMESH-t=tools-page=1
It is possible to enable the internal IIS3DWB high pass filter (HPF), this option then removes the DC component of the acceleration - the earth gravity. In the webinar we mentioned MotionSP middleware (FP-IND-PREDMNT1), which outputs RMS speed direct...
There are several SW project examples written in C code for STWIN and also different IDEs can be used, STM32CubeIDE, IAR, Keil. ST-Link V3 programming probe is also part of STWIN development kit for programming and debugging purposes. Both STSW-STWIN...