cancel
Showing results for 
Search instead for 
Did you mean: 

Question from Predictive Maintenance Webinar 29th of April: Can we measure electrical signature using magnetometer in STWIN kit?

Pasi MYLLYMAKI
ST Employee
 
1 REPLY 1
Vladimir  JANOUSEK
Associate II

Yes, this is possible. IIS2MDC is potentially the product which can be considered. It Is important to respect the magnetic field strenght vs. IIS2MDC measurement range, and if the sampling speed is sufficient for particular application (150Hz max) etc.