2015-12-22 5:58 PM
Hi,
I would like to use the osxMotionFX for the STM32L053 Nucleo board I have. Any plan for a release? It seems to be working only on Nucleo F401RE. Also when I install the osxMotion Setup V1.4.0, I get an error message during the license wizard installation ''floating point 0''. Anyone had the same issue? Thanks, Pierre2016-07-14 8:36 AM
Hello,
just NUCLEO-F401RE or NUCLEO-L476RG boards are supported so far.
BR,
Marian