cancel
Showing results for 
Search instead for 
Did you mean: 

On GitHub there are two MLC examples for wrist-tilt recognition, one that uses gyro + accelerometer and one that uses only XL. Why?

Eleon BORLINI
ST Employee
 
1 ACCEPTED SOLUTION

Accepted Solutions
Eleon BORLINI
ST Employee

The difference lies in the accuracy of the two models, the MLC without gyro helps the user to save some power consumption but, as a tradeoff, will provide a worse performance of wrist-tilt detection if compared to the one w/ gyroscope.

View solution in original post

1 REPLY 1
Eleon BORLINI
ST Employee

The difference lies in the accuracy of the two models, the MLC without gyro helps the user to save some power consumption but, as a tradeoff, will provide a worse performance of wrist-tilt detection if compared to the one w/ gyroscope.