2024-11-28 7:21 AM
I am trying to do USB sensor data streaming Real Time Plot by conecting my steval mkboxpro with hsdatalog_GUI.py but it keeps saying "Device Template Model Loading". Anyone can help?
Thanks
Solved! Go to Solution.
2024-12-04 12:56 AM
Hi @FilipeLourenço ,
The HSDPython_SDK is compatible only with FP-SNS-DATALOG2 fw flashed on sensortile.box Pro board.
you can download the fw tools here
hsdatalog_GUI.py works within the HSDPython_SDK, developed in Python 3.10 on Windows and Linux
environments.
HSDPython_SDK requires different Python modules, distributed together with FP-SNS-DATALOG2.
By installing them through the provided installers, all the required dependencies are automatically solved – see HSDPython_SDK to fully setup your Python environment.
Execute hsdatalog_GUI.py
Once the board is connected via USB and the Python environment has been properly updated, you can launch the real time plot by just executing hsdatalog_GUI.py available in Utilities/HSDPython_SDK/examples
To execute the script you can open a command shell there and run python hsdatalog_GUI.py
2024-12-04 12:56 AM
Hi @FilipeLourenço ,
The HSDPython_SDK is compatible only with FP-SNS-DATALOG2 fw flashed on sensortile.box Pro board.
you can download the fw tools here
hsdatalog_GUI.py works within the HSDPython_SDK, developed in Python 3.10 on Windows and Linux
environments.
HSDPython_SDK requires different Python modules, distributed together with FP-SNS-DATALOG2.
By installing them through the provided installers, all the required dependencies are automatically solved – see HSDPython_SDK to fully setup your Python environment.
Execute hsdatalog_GUI.py
Once the board is connected via USB and the Python environment has been properly updated, you can launch the real time plot by just executing hsdatalog_GUI.py available in Utilities/HSDPython_SDK/examples
To execute the script you can open a command shell there and run python hsdatalog_GUI.py
2024-12-11 6:49 AM
Hi, @Federica Bossi
Thanks for the Help.
I already have the FP-SNS-DATALOG2 fw flashed on sensortile.box Pro board, Python 3.12 installed, and the HSDPython_SDK installed.
But when i execute hsdatalog_GUI.py it detects the board, but keeps giving the message "Device Template Model Loading"
Do you have any other recommendation?
2024-12-11 7:08 AM
I wanted to use the hsdatalog_GUI.py to see the real time plot of the acc and mic measurements, because i am getting negative timestamps in the data from microSD. I don't know if it is because of the files from the SDcard or because of the .dat to .csv file conversion done.
When i used the normal fw from the mkboxpro everything was ok, but the files that i got from the SDcard was .csv. Now, with the high speed data logging, the files are .dat and after the conversion i am getting very low timestamps like 1^-12, and a lot of negative timestamps.